EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EI_API_CIP_SAttr Struct Reference

General attribute parameter collection. More...

#include <EI_API_CIP_define.h>

Data Fields

uint16_t id
 
EI_API_CIP_EEdt_t edt
 
EI_API_CIP_ECdt_t cdt
 
EI_API_CIP_EAr_t accessRule
 
uint16_t edtSize
 
uint16_t cdtSize
 
uint16_t index
 
void * pvValue
 
EI_API_CIP_CBGetAttr get_callback
 
EI_API_CIP_CBGetAttr_CIPRouting get_callback_routed
 
EI_API_CIP_CBSetAttr set_callback
 
EI_API_CIP_CBSetAttr_CIPRouting set_callback_routed
 

Detailed Description

General attribute parameter collection.