EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EI_API_CIP_SAssemMapData Struct Reference

Data structure used during callback in custom-map assemblies. More...

#include <EI_API_def.h>

Data Fields

uint16_t classId
 
uint16_t instanceId
 
uint16_t attributeId
 
uint8_t * pAttribBuf
 

Detailed Description

Data structure used during callback in custom-map assemblies.