EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ maxInstanceNum

uint16_t maxInstanceNum

Maximum number of instances defined in CIP object dictionary. Please be aware that minimum value is defined for this parameter. It is depended on number of common classes/instances created by default by the stack. Minimum value is defined by EI_API_CIP_OBD_MIN macro in EI_API_def.h header file.