EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EI_API_ADP_SParam Struct Reference

#include <EI_API_ADP_define.h>

Data Fields

uint8_t len
 
uint8_t * data
 

Detailed Description

Structure to use as function parameter (see adapter setter and getter functions).