EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ msgTxInterval

uint16_t msgTxInterval

From IEEE 802.1AB-2016, 9.2.5.7. The interval in seconds at which LLDP frames are transmitted from this device.