#include <EI_API_ADP_define.h>
Data Fields | ||
| OSAL_TASK_Priority_t | taskPrioCyclicIo | |
| OSAL_TASK_Priority_t | taskPrioPacket | |
| OSAL_TASK_Priority_t | taskPrioStatistic | |
| struct { | ||
| struct { | ||
| OSAL_TASK_Priority_t taskPrioTsDelayRqTx | ||
| OSAL_TASK_Priority_t taskPrioTxTimeStamp | ||
| OSAL_TASK_Priority_t taskPrioNRT | ||
| OSAL_TASK_Priority_t taskPrioBackground | ||
| uint32_t timeSyncRxPhyLatency | ||
| uint32_t timeSyncTxPhyLatency | ||
| uint32_t timeSyncIEPClkFreq | ||
| } ptp | ||
| struct { | ||
| OSAL_TASK_Priority_t taskPrioReceive | ||
| uint16_t maxNeighborDevices | ||
| } lldp | ||
| } | dll | |