EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EI_API_ADP_SCurrentIpData Struct Reference

#include <EI_API_ADP_define.h>

Data Fields

EIP_EConfigurationMethod_t configurationMethod
 
uint32_t ipAddr
 
uint32_t networkMask
 
uint32_t gatewayAdress
 
uint32_t nameServer1
 
uint32_t nameServer2
 
char domainName [EI_API_CIP_DOMAIN_NAME_LENGTH+1]