Definition for ConnectionManager callback functions. More...
#include <EI_API_def.h>
Data Fields | |
| uint8_t | prioTimeTick |
| uint8_t | timeOutTicks |
| uint32_t | o2tNwConId |
| uint32_t | t2oNwConId |
| uint16_t | conSerialNum |
| uint16_t | orgVendorId |
| uint32_t | orgSerialNum |
| uint8_t | timeOutMulti |
| uint32_t | o2tRPI |
| uint32_t | o2tConPara |
| uint32_t | t2oRPI |
| uint32_t | t2oConPara |
| uint8_t | typeTrigger |
| uint8_t | conPathSize |
| uint8_t | conPath [EI_API_ADP_CMGR_CONNECTION_SIZE_MAX] |
Definition for ConnectionManager callback functions.
Information from the ForwardOpen, LargeForwardOpen or ForwardClose message