EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
EI_API_ADP_SCmgrForwardCloseInfo Struct Reference

#include <EI_API_def.h>

Data Fields

uint8_t prioTimeTick
 
uint8_t timeOutTicks
 
uint16_t conSerialNum
 
uint16_t orgVendorId
 
uint32_t orgSerialNum
 
uint8_t conPathSize
 
uint8_t conPath [EI_API_ADP_CMGR_CONNECTION_SIZE_MAX]