EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
DIO_DEVICE_DOP_object Struct Reference

Data Fields

uint16_t instanceID
 
DIO_DEVICE_DOP_ObjectCfg_t userCfg
 
volatile bool faultSettingChanged
 
volatile bool idleSettingChanged
 
volatile bool runIdleValueChanged
 
volatile bool receiveDataEvent
 
volatile bool receiveIdleEvent
 
DIO_DEVICE_DOP_Value_t valueContainer
 
volatile ei_api_cip_edt_bool run_idle_command
 
volatile DIO_DEVICE_DOP_SmStates_t current_state
 
volatile DIO_DEVICE_DOP_SmStates_t old_state
 
void(* processesFnc )(struct DIO_DEVICE_DOP_object *, DIO_DEVICE_DOP_events_t)
 
struct DIO_DEVICE_DOP_objectnextObject