EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
DEVICE_PROFILE_CFG_SInit Struct Reference

Initialization parameters of non-volatile configuration data. More...

#include <device_profile_cfg.h>

Data Fields

DEVICE_PROFILE_NVM_EType_t type
 
uint32_t instance
 
uint32_t address
 

Detailed Description

Initialization parameters of non-volatile configuration data.