EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
DEVICE_PROFILE_CFG_AdapterData Struct Reference

#include <device_profile_cfg.h>

Data Fields

uint32_t ipAddr
 
uint32_t ipNwMask
 
uint32_t ipGateway
 
uint32_t nameServer1
 
uint32_t nameServer2
 
char aDomainName [48]
 
uint8_t configurationMethod
 
char aHostName [64]
 
uint8_t ttlValue
 
bool acdActive
 
uint8_t acdState
 
uint8_t aAcdAddr [6]
 
uint8_t aAcdHdr [28]
 
uint16_t encapInactTimeout
 
EI_API_ADP_UIntfConf_t intfConfig [2]
 
bool ptpEnable
 
bool portEnable
 
uint16_t portLogAnnounceInterval
 
int16_t portLogSyncInterval
 
uint8_t domainNumber
 
char aUserDescription [128]
 
EI_API_ADP_SQos_t qosParameter
 
EI_API_ADP_SMcastConfig_t mcastConfig
 
bool quickConnectEnabled
 
EI_API_ADP_SLldp_Parameter_t lldpParameter