EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ GENERIC_DEVICE_cipGenerateContent()

static void GENERIC_DEVICE_cipGenerateContent ( EI_API_CIP_NODE_T *  cipNode,
uint16_t  classId,
uint16_t  instanceId 
)
static

Generates attributes and services for a CIP™class.

Create a CIP class with a Class IDs using the value specified in parameter classId.
Generates attributes and services for that class.
Adds read and write services.
Adds 64 8-bit attributes with callback function.
Adds 32 16-bit attributes.
Adds 16 32-bit attributes.
Adds 8 64-bit attributes.