#include "device_profiles/generic_device/generic_device_cfg.h"
{
if (NULL == pAdapter)
{
goto laError;
}
...
laError:
{
OSAL_error (__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
}
return;
}
@ EI_API_ADP_eERR_GENERAL
Definition EI_API_ADP_define.h:47
@ EI_API_ADP_eERR_OK
Definition EI_API_ADP_define.h:46
void GENERIC_DEVICE_CFG_apply(EI_API_ADP_T *pAdapter)
Applies the generic device profile configuration data on stack.
Definition generic_device_cfg.c:208
static uint32_t GENERIC_DEVICE_CFG_applyTimeSync(EI_API_ADP_T *pAdapter)
Applies the Time Sync object attributes on the stack.
Definition generic_device_cfg.c:754