#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId = 0x10D;
uint8_t maxLinkAddr = 8,
const uint8_t routablePorts[] = {11, 7, 3};
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition EI_API_CIP_stub.c:215
ETHIP_API uint32_t EI_API_CIP_setRoutingMaxLinkAddr(T *pCipNode_p, uint8_t linkAddr_p)
Initialize a maximum number of link addresses used by application.
Definition EI_API_CIP_stub.c:5457
ETHIP_API uint32_t EI_API_CIP_setRoutingRoutablePorts(T *pCipNode_p, const uint8_t *pRoutablePortTable_p, uint8_t mapsize_p)
Provides setup of routable ports.
Definition EI_API_CIP_stub.c:5609
ETHIP_API T * EI_API_CIP_NODE_new(EI_API_CIP_NODE_InitParams_t *pInitParams)
Create a new CIP node.
Definition EI_API_CIP_stub.c:81
uint16_t maxInstanceNum
Definition EI_API_CIP_define.h:162
Initialization parameters to create new CIP Node.
Definition EI_API_CIP_define.h:161