#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId = 0x0064;
uint16_t instanceId = 0x01;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition EI_API_CIP_stub.c:215
@ EI_API_CIP_eAR_GET
Attribute is gettable.
Definition EI_API_def.h:123
@ EI_API_CIP_eEDT_UINT
Definition EI_API_CIP_define.h:98
@ EI_API_CIP_eCDT_NO
Definition EI_API_CIP_define.h:133
ETHIP_API uint32_t EI_API_CIP_cloneInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t instanceIdSrc_p)
Clone attributes from source instance to a another/new instance.
Definition EI_API_CIP_stub.c:1393
ETHIP_API uint32_t EI_API_CIP_createInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p)
Creates a CIP instance.
Definition EI_API_CIP_stub.c:787
ETHIP_API uint32_t EI_API_CIP_addInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Add an attribute to an instance.
Definition EI_API_CIP_stub.c:1170
ETHIP_API T * EI_API_CIP_NODE_new(EI_API_CIP_NODE_InitParams_t *pInitParams)
Create a new CIP node.
Definition EI_API_CIP_stub.c:81
uint16_t maxInstanceNum
Definition EI_API_CIP_define.h:162
Initialization parameters to create new CIP Node.
Definition EI_API_CIP_define.h:161
EI_API_CIP_EEdt_t edt
Definition EI_API_CIP_define.h:186
EI_API_CIP_EAr_t accessRule
Definition EI_API_CIP_define.h:188
uint16_t id
Definition EI_API_CIP_define.h:185
EI_API_CIP_ECdt_t cdt
Definition EI_API_CIP_define.h:187
uint16_t cdtSize
Definition EI_API_CIP_define.h:190
uint16_t edtSize
Definition EI_API_CIP_define.h:189
General attribute parameter collection.
Definition EI_API_CIP_define.h:184