EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_CIP_CBGetAttr_CIPRouting

typedef uint32_t(* EI_API_CIP_CBGetAttr_CIPRouting) (EI_API_CIP_NODE_T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, uint16_t *len_p, void *pvValue_p, uint16_t linkAddress_p)

Function prototype for CIP get attribute callback function for Routed objects.