| uint32_t EI_API_CIP_setAttr_uint | ( | T * | pCipNode_p, |
| uint16_t | classId_p, | ||
| uint16_t | instanceId_p, | ||
| uint16_t | attrId_p, | ||
| ei_api_cip_edt_uint | attrValue_p | ||
| ) |
Set attribute of type UINT.
This function that sets the attribute value of the CIP specified elementary data type UINT. If the operation is completed successfully, the function returns EI_API_CIP_eERR_OK, else an error code.
| [in] | pCipNode_p | Pointer to the CIP node. |
| [in] | classId_p | Class identifier. |
| [in] | instanceId_p | Instance identifier. |
| [in] | attrId_p | Attribute identifier. |
| [in] | attrValue_p | The new attribute value. |
| EI_API_CIP_eERR_OK | Success. |
| EI_API_CIP_eERR_NODE_INVALID | CIP node is invalid, possibly EI_API_CIP_NODE_new() was not called. |
| EI_API_CIP_eERR_CLASS_DOES_NOT_EXIST | Class does not exists in CIP node dictionary. |
| EI_API_CIP_eERR_INSTANCE_DOES_NOT_EXIST | Instance does not exist in CIP node dictionary. |
| EI_API_CIP_eERR_ATTRIBUTE_DOES_NOT_EXIST | Attribute does not exist in class or instance. |
| EI_API_CIP_eERR_ATTRIBUTE_INVALID_VALUE | Invalid data pointer |
| EI_API_CIP_eERR_ATTRIBUTE_INVALID_TYPE | Attribute type is invalid. |
| EI_API_CIP_eERR_ATTRIBUTE_UNKNOWN_STATE | Unknown state during attribute operation reached. |