EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_CIP_setAttr_lword()

uint32_t EI_API_CIP_setAttr_lword ( T *  pCipNode_p,
uint16_t  classId_p,
uint16_t  instanceId_p,
uint16_t  attrId_p,
ei_api_cip_edt_lword  attrValue_p 
)

Set attribute of type LWORD.

This function sets the attribute value of the CIP specified elementary data type LWORD. If the operation is completed successfully, the function returns EI_API_CIP_eERR_OK, else an error code.

Parameters
[in]pCipNode_pPointer to the CIP node.
[in]classId_pClass identifier.
[in]instanceId_pInstance identifier.
[in]attrId_pAttribute identifier.
[in]attrValue_pThe new attribute value.
Returns
EI_API_CIP_EError_t as uint32_t value.
Return values
EI_API_CIP_eERR_OKSuccess.
EI_API_CIP_eERR_NODE_INVALIDCIP node is invalid, possibly EI_API_CIP_NODE_new() was not called.
EI_API_CIP_eERR_CLASS_DOES_NOT_EXISTClass does not exists in CIP node dictionary.
EI_API_CIP_eERR_INSTANCE_DOES_NOT_EXISTInstance does not exist in CIP node dictionary.
EI_API_CIP_eERR_ATTRIBUTE_DOES_NOT_EXISTAttribute does not exist in class or instance.
EI_API_CIP_eERR_ATTRIBUTE_INVALID_VALUEInvalid data pointer.
EI_API_CIP_eERR_ATTRIBUTE_INVALID_TYPEAttribute type is invalid.
EI_API_CIP_eERR_ATTRIBUTE_UNKNOWN_STATEUnknown state during attribute operation reached.
Example
#include "EI_API.h"
// Elementary data type LWORD
ei_api_cip_edt_lword attrLwordValue = 0x1515616115156161;
uint32_t errCode;
classId = 0x0064;
instanceId = 0x0001;
attrId = 0x0002;
// Set attribute with identifier 0x0002 from class 0x0064 and instance 0x0001 to 0x1515616115156161
errCode = EI_API_CIP_setAttr_lword(pEI_API_CIP_NODE, classId, instanceId, attrId, attrLwordValue);
ETHIP_API uint32_t EI_API_CIP_setAttr_lword(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lword value_p)
Set attribute of type LWORD.
Definition EI_API_CIP_stub.c:4223
See also
EI_API_CIP_getAttr_lword ei_api_cip_edt_lword EI_API_CIP_EError_t