#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t linkAddr = 1,
uint16_t assemblyInstanceId;
...
assemblyInstanceId = 0xc1;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_CIP_createRoutingAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p, uint8_t linkAddr_p)
Create a new routable assembly instance.
Definition EI_API_CIP_stub.c:6316
@ EI_API_CIP_eAR_GET_AND_SET
Definition EI_API_def.h:124
ETHIP_API T * EI_API_CIP_NODE_new(EI_API_CIP_NODE_InitParams_t *pInitParams)
Create a new CIP node.
Definition EI_API_CIP_stub.c:81
uint16_t maxInstanceNum
Definition EI_API_CIP_define.h:162
Initialization parameters to create new CIP Node.
Definition EI_API_CIP_define.h:161