#include "EI_API.h"
uint32_t EI_APP_cfgAssemblyCb (EI_API_CIP_NODE_T* pCipNode_p,
uint16_t o2t_p,
uint16_t t2o_p,
uint16_t cfg_inst_p,
const uint8_t* const cfg_data_p,
uint16_t cfg_data_size_p)
{
}
void EI_APP_cipInit (void)
{
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t cfgAssemblyInstanceId;
...
cfgAssemblyInstanceId = 0x67;
...
}
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_CIP_setCfgAssemblyCb(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssemblySimple fuCfgAssemblyAccess_p)
Set configuration assembly callback.
Definition EI_API_CIP_stub.c:5380
ETHIP_API uint32_t EI_API_CIP_createCfgAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssembly fuCfgAssemblyAccess_p)
Creates configuration assembly instance under Assembly Object class.
Definition EI_API_CIP_stub.c:5244
@ EI_API_eERR_CB_NO_ERROR
Definition EI_API_def.h:147
ETHIP_API T * EI_API_CIP_NODE_new(EI_API_CIP_NODE_InitParams_t *pInitParams)
Create a new CIP node.
Definition EI_API_CIP_stub.c:81
uint16_t maxInstanceNum
Definition EI_API_CIP_define.h:162
Initialization parameters to create new CIP Node.
Definition EI_API_CIP_define.h:161