#include "EI_API.h"
uint32_t EI_APP_cfgAssemblyCb (EI_API_CIP_NODE_T* pCipNode_p,
uint16_t o2t_p,
uint16_t t2o_p,
uint16_t cfg_inst_p,
const uint8_t* const cfg_data_p,
uint16_t cfg_data_size_p)
{
}
void EI_APP_cipInit (void)
{
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId;
uint16_t instanceId;
uint16_t attrId;
uint16_t cfgAssemblyInstanceId;
...
classId = 0x70;
instanceId = 0x01;
attrId = 0x300;
uint8_t value = 0xFF;
cfgAssemblyInstanceId = 0x67;
...
}
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_CIP_setCfgAssemblyCb(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssemblySimple fuCfgAssemblyAccess_p)
Set configuration assembly callback.
Definition EI_API_CIP_stub.c:5380
ETHIP_API uint32_t EI_API_CIP_addAssemblyMember(T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attributeId_p)
Add an member to an assembly member list.
Definition EI_API_CIP_stub.c:4435
ETHIP_API uint32_t EI_API_CIP_createCfgAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssembly fuCfgAssemblyAccess_p)
Creates configuration assembly instance under Assembly Object class.
Definition EI_API_CIP_stub.c:5244
ETHIP_API uint32_t EI_API_CIP_addClassService(T *pCipNode_p, uint16_t classId_p, EI_API_CIP_SService_t *pService_p)
Add service/s to the class.
Definition EI_API_CIP_stub.c:292
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition EI_API_CIP_stub.c:215
@ EI_API_CIP_eSC_GETATTRSINGLE
Definition EI_API_def.h:109
@ EI_API_CIP_eSC_SETATTRSINGLE
Definition EI_API_def.h:110
@ EI_API_CIP_eAR_GET_AND_SET
Definition EI_API_def.h:124
@ EI_API_CIP_eEDT_USINT
Definition EI_API_CIP_define.h:97
@ EI_API_CIP_eCDT_NO
Definition EI_API_CIP_define.h:133
@ EI_API_eERR_CB_NO_ERROR
Definition EI_API_def.h:147
ETHIP_API uint32_t EI_API_CIP_createInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p)
Creates a CIP instance.
Definition EI_API_CIP_stub.c:787
ETHIP_API uint32_t EI_API_CIP_addInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Add an attribute to an instance.
Definition EI_API_CIP_stub.c:1170
ETHIP_API uint32_t EI_API_CIP_setInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Set instance attribute value only.
Definition EI_API_CIP_stub.c:1592
ETHIP_API T * EI_API_CIP_NODE_new(EI_API_CIP_NODE_InitParams_t *pInitParams)
Create a new CIP node.
Definition EI_API_CIP_stub.c:81
uint16_t maxInstanceNum
Definition EI_API_CIP_define.h:162
Initialization parameters to create new CIP Node.
Definition EI_API_CIP_define.h:161
EI_API_CIP_EEdt_t edt
Definition EI_API_CIP_define.h:186
EI_API_CIP_EAr_t accessRule
Definition EI_API_CIP_define.h:188
uint16_t id
Definition EI_API_CIP_define.h:185
EI_API_CIP_ECdt_t cdt
Definition EI_API_CIP_define.h:187
uint16_t cdtSize
Definition EI_API_CIP_define.h:190
void * pvValue
Definition EI_API_CIP_define.h:192
General attribute parameter collection.
Definition EI_API_CIP_define.h:184
EI_API_CIP_ESc_t code
Definition EI_API_CIP_define.h:173
EI_API_CIP_CBService callback
Definition EI_API_CIP_define.h:176
uint16_t getAttrAllResponseCnt
Definition EI_API_CIP_define.h:174
General service parameter collection.
Definition EI_API_CIP_define.h:172