EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_CIP_setAssemblyAppType()

uint32_t EI_API_CIP_setAssemblyAppType ( T *  pCipNode_p,
uint16_t  assemblyInstanceId_p,
EI_API_CIP_EAPP_TYPE_t  appType_p 
)

Apply an application type to an existing assembly instance.

This function applies an application type to an existing assembly instance.

Parameters
[in]pCipNode_pPointer to the CIP node.
[in]assemblyInstanceId_pInstance identifier.
[in]appType_pThe application type to be applied
Returns
EI_API_CIP_EError_t as uint32_t value.
Return values
EI_API_CIP_eERR_OKSuccess.
EI_API_CIP_eERR_ASSEMBLY_DOES_NOT_EXISTThe given instance id does not exist in the assembly object
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t assemblyInstanceId;
// Create a new adapter first
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Create a CIP node next
initParams.maxInstanceNum = 256;
pEI_API_CIP_NODE = EI_API_CIP_NODE_new(&initParams);
...
// Under pEI_API_CIP_NODE, create assembly instance with ID = 193, with read-write access and
// application type 'Input Only'
assemblyInstanceId = 0xc1;
errCode = EI_API_CIP_createAssembly(pEI_API_CIP_NODE, assemblyInstanceId, EI_API_CIP_eAR_GET_AND_SET);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_CIP_setAssemblyAppType(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAPP_TYPE_t appType_p)
Apply an application type to an existing assembly instance.
Definition EI_API_CIP_stub.c:5145
ETHIP_API uint32_t EI_API_CIP_createAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p)
Create a new assembly instance.
Definition EI_API_CIP_stub.c:4312
@ EI_API_CIP_eAPP_TYPE_IO
Input Only.
Definition EI_API_def.h:137
@ EI_API_CIP_eAR_GET_AND_SET
Definition EI_API_def.h:124
ETHIP_API T * EI_API_CIP_NODE_new(EI_API_CIP_NODE_InitParams_t *pInitParams)
Create a new CIP node.
Definition EI_API_CIP_stub.c:81
uint16_t maxInstanceNum
Definition EI_API_CIP_define.h:162
Initialization parameters to create new CIP Node.
Definition EI_API_CIP_define.h:161
See also
EI_API_CIP_createAssembly EI_API_CIP_addAssemblyMember EI_API_CIP_getAssemblySize EI_API_CIP_getAssemblyData EI_API_CIP_setAssemblyData EI_API_CIP_EAr_t EI_API_CIP_EError_t