|
| uint32_t | EI_API_CIP_createAssembly (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p) |
| | Create a new assembly instance.
|
| |
| uint32_t | EI_API_CIP_addAssemblyMember (T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attributeId_p) |
| | Add an member to an assembly member list.
|
| |
| uint32_t | EI_API_CIP_addAssemblyMemberCustomMapped (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_SAssemCustomMap_t *pCustomAssembMap) |
| | Add a member to an assembly member list with customized mapping.
|
| |
| uint32_t | EI_API_CIP_getAssemblySize (T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t *pSize_p) |
| | Get assembly instance attribute Size.
|
| |
| uint32_t | EI_API_CIP_getAssemblyData (T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pDestinationBuffer_p, uint16_t destinationBufferLength_p) |
| | Get assembly instance attribute data.
|
| |
| uint32_t | EI_API_CIP_setAssemblyData (T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pSourceBuffer_p, uint16_t sourceBufferLength_p) |
| | Set assembly instance attribute data.
|
| |
| uint32_t | EI_API_CIP_setAssemblyFormat (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAssemb_Format_t format_p) |
| | Set assembly format.
|
| |
| uint32_t | EI_API_CIP_setAssemblyAppType (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAPP_TYPE_t appType_p) |
| | Apply an application type to an existing assembly instance.
|
| |
| uint32_t | EI_API_CIP_createCfgAssembly (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssembly fuCfgAssemblyCb_p) |
| | Creates configuration assembly instance under Assembly Object class.
|
| |
| uint32_t | EI_API_CIP_setCfgAssemblyCb (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssemblySimple fuCfgAssemblyCb_p) |
| | Set configuration assembly callback.
|
| |
| uint32_t | EI_API_CIP_createRoutingCfgAssembly (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_CBCfgAssembly fuCfgAssemblyCb_p, uint8_t linkAddress_p) |
| | Creates routed configuration assembly instance under Assembly Object class.
|
| |
| uint32_t | EI_API_CIP_createRoutingAssembly (T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p, uint8_t linkAddr_p) |
| | Create a new routable assembly instance.
|
| |
| uint32_t | EI_API_CIP_getRoutingAssemblySize (T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t *pSize_p, uint8_t linkAddr_p) |
| | Get routable assembly instance attribute Size.
|
| |
| uint32_t | EI_API_CIP_getRoutingAssemblyData (T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pDestinationBuffer_p, uint16_t destinationBufferLength_p, uint8_t linkAddr_p) |
| | Get routable assembly instance attribute data.
|
| |
| uint32_t | EI_API_CIP_setRoutingAssemblyData (T *pCipNode_p, uint16_t assemblyInstanceId_p, void *pSourceBuffer_p, uint16_t sourceBufferLength_p, uint8_t linkAddr_p) |
| | Set routable assembly instance attribute data.
|
| |
| uint32_t | EI_API_CIP_addRoutingAssemblyMember (T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attributeId_p, uint8_t linkAddr_p) |
| | Add an member to an routable assembly member list.
|
| |