EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_getPortEnable()

uint32_t EI_API_ADP_getPortEnable ( T *  pAdp_p,
bool *  pPortEnable_p 
)

Get the PortEnable attribute state of the Time Sync Object (Instance Attribute ID: 13).

Function that returns the PortEnable member of the PortEnableCfg attribute for the EtherNet/IP adapter selected by parameter pAdp_p in output parameter pPortEnable.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pPortEnable_pPointer to a boolean that is set to true if a PTP port is enabled and false if not.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
bool portEnable;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getPortEnable(pEI_API_ADP, &portEnable);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_getPortEnable(T *pAdp_p, bool *pPortEnable_p)
Get the PortEnable attribute state of the Time Sync Object (Instance Attribute ID: 13).
Definition EI_API_ADP_stub.c:1656
See also
EI_API_ADP_setPortEnable EI_API_ADP_EError_t