| uint32_t EI_API_ADP_getTimeSyncManufactureID | ( | T * | pAdp_p, |
| char * | pManufactureID_p | ||
| ) |
Get the ManufactureIdentity attribute of the Time Sync Object (Instance Attribute ID: 20).
Function that returns the ManufactureIdentity attribute of the Time Sync Object for the adapter selected by parameter pAdp_p in output parameter pManufactureID_p.
| [in] | pAdp_p | Pointer to the adapter. |
| [out] | pManufactureID_p | char pointer to ManufactureIdentity of the adapter Time Sync object specified by parameter pAdp_p. |
| EI_API_ADP_eERR_OK | Success. |
| EI_API_ADP_eERR_GENERAL | General error. |