EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_setACD()

uint32_t EI_API_ADP_setACD ( T *  pAdp_p,
bool  enable_p 
)

Enable or disable address conflict detection (Instance Attribute ID: 10).

Function that allows to enable or disable Address Conflict Detection (ACD).

Parameters
[in]pAdp_pPointer to the adapter.
[in]enable_pBoolean flag which enables or disables the ACD functionality.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_setACD(pEI_API_ADP, true);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_setACD(T *pAdp_p, bool enable_p)
Enable or disable address conflict detection (Instance Attribute ID: 10).
Definition EI_API_ADP_stub.c:3832
See also
EI_API_ADP_getACD EI_API_ADP_EError_t