| uint32_t EI_API_ADP_getACD | ( | T * | pAdp_p, |
| bool * | pAcdEnabled_p | ||
| ) |
Get the current address conflict detection setting (Instance Attribute ID: 10).
This function returns a boolean value indicating if Address Conflict Detection (ACD) is enabled or disabled.
| [in] | pAdp_p | Pointer to the adapter. |
| [out] | pAcdEnabled_p | Pointer to a boolean parameter that indicates if ACD is enabled. |
| EI_API_ADP_eERR_OK | Success. |
| EI_API_ADP_eERR_GENERAL | General error. |