#include "EI_API.h"
#include "EI_API_def.h"
char *methodName[3] = { "static", "bootp", "dhcp" };
EI_API_ADP_getCurrentIpData(pAdapter, ¤tIpData);
OSAL_printf("confMethod %s ip %x mask %x gw %x ns1 %x ns2 %x domainname %s\r\n",
EIP_EConfigurationMethod_t configurationMethod
Definition EI_API_ADP_define.h:242
uint32_t ipAddr
Definition EI_API_ADP_define.h:243
uint32_t nameServer1
Definition EI_API_ADP_define.h:246
uint32_t gatewayAdress
Definition EI_API_ADP_define.h:245
uint32_t networkMask
Definition EI_API_ADP_define.h:244
uint32_t nameServer2
Definition EI_API_ADP_define.h:247
char domainName[EI_API_CIP_DOMAIN_NAME_LENGTH+1]
Definition EI_API_ADP_define.h:248
Definition EI_API_ADP_define.h:241