| uint32_t EI_API_ADP_setQuickConnectSupported | ( | T * | pAdp_p | ) |
Enable QuickConnect support.
Enable QuickConnect support. This function should only be used for EtherNet/IP QuickConnect applications.
| [in] | pAdp_p | Pointer to the adapter. |
| EI_API_ADP_eERR_OK | Success. |
| EI_API_ADP_eERR_GENERAL | General error. |