EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_setEnipAcdHdr()

uint32_t EI_API_ADP_setEnipAcdHdr ( T *  pAdp_p,
const EI_API_ADP_SParam_t pEnipAcdHdr_p 
)

Set the address conflict detection header (Instance Attribute ID: 11).

Function to set the current Address Conflict Detection (ACD) header.

Parameters
[in]pAdp_pPointer to the adapter.
[in]pEnipAcdHdr_pPointer to the ACD header packed within a EI_API_ADP_SParam_t type.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
EI_API_ADP_eERR_LENGTHIllegal parameter length.
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint8_t acdHeader[28];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Fill your ACD header before passing
for (uint8_t i = 0; i <= 27)
{
acdHeader[i] = 0x00;
}
// reset ACD header
errCode = EI_API_ADP_setEnipAcdAddr(pEI_API_ADP, acdHeader);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_setEnipAcdAddr(T *pAdp_p, const EI_API_ADP_SParam_t *pEnipAcdAddr_p)
Set the address conflict detection MAC address (Instance Attribute ID: 11).
Definition EI_API_ADP_stub.c:4065
See also
EI_API_ADP_getEnipAcdAddr EI_API_ADP_EError_t