#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
printf("EI_API_ADP_getQoS - Error Code: %08x\n \
- Q_Tag_Enable: %d\n \
- DSCP_Urgent: %d\n \
- DSCP_Scheduled: %d\n \
- DSCP_High: %d\n \
- DSCP_Low: %d\n \
- DSCP_Explicit: %d\n\n",
errCode,
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_getQoS(T *pAdp_p, EI_API_ADP_SQos_t *pQoS_p)
Get the current QoS settings (Instance Attribute IDs: 4 - 8).
Definition EI_API_ADP_stub.c:2661
uint8_t Q_Tag_Enable
Definition EI_API_def.h:262
uint8_t DSCP_High
Definition EI_API_def.h:267
uint8_t DSCP_Explicit
Definition EI_API_def.h:269
uint8_t DSCP_Scheduled
Definition EI_API_def.h:266
uint8_t DSCP_Urgent
Definition EI_API_def.h:265
uint8_t DSCP_Low
Definition EI_API_def.h:268
General QoS attribute parameter collection.
Definition EI_API_def.h:261