EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_getRevision()

uint32_t EI_API_ADP_getRevision ( T *  pAdp_p,
EI_API_ADP_SRevision_t pRevision_p 
)

Get the adapter Revision (Instance Attribute ID: 4).

Function that returns the revision of the adapter selected by parameter pAdp_p. The revision attribute is divided into major and minor revision number.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pRevision_pPointer to an adapter revision structure.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getRevision(pEI_API_ADP, &revision);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_getRevision(T *pAdp_p, EI_API_ADP_SRevision_t *pRevision_p)
Get the adapter Revision (Instance Attribute ID: 4).
Definition EI_API_ADP_stub.c:1000
Definition EI_API_ADP_define.h:100
See also
EI_API_ADP_setRevision EI_API_ADP_SRevision_t EI_API_ADP_EError_t