#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_setRevision(T *pAdp_p, EI_API_ADP_SRevision_t revison_p)
Set the adapter Revision (Instance Attribute ID: 4).
Definition EI_API_ADP_stub.c:1063
uint8_t major
Definition EI_API_ADP_define.h:101
uint8_t minor
Definition EI_API_ADP_define.h:103
Definition EI_API_ADP_define.h:100