EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_getMacAddr()

uint32_t EI_API_ADP_getMacAddr ( T *  pAdp_p,
EI_API_ADP_SParam_t pMacAddr_p 
)

Get the adapter MAC address (Instance Attribute ID: 3).

Function that returns the current adapter MAC address.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pMacAddr_pPointer to the MAC address packed within a EI_API_ADP_SParam_t type.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getMacAddr(pEI_API_CIP_ADP, &macAddr);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
ETHIP_API uint32_t EI_API_ADP_getMacAddr(T *pAdp_p, EI_API_ADP_SParam_t *pMacAddr_p)
Get the adapter MAC address (Instance Attribute ID: 3).
Definition EI_API_ADP_stub.c:4647
Definition EI_API_ADP_define.h:85
See also
EI_API_ADP_SParam_t EI_API_ADP_EError_t