EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_EError

ADP error codes (base 0x38020Axx).

Enumerator
EI_API_ADP_eERR_OK 

No error, everything should be fine.

EI_API_ADP_eERR_GENERAL 

General ADP error.

EI_API_ADP_eERR_NOT_IMPLEMENTED 

Adapter function not implemented.

EI_API_ADP_eERR_LENGTH 

Length error.

EI_API_ADP_eERR_MEMALLOC 

Error during memory allocation.

EI_API_ADP_eERR_STUB_INVALIDPARAMETER 

Invalid parameter populate interface.

EI_API_ADP_eERR_STUB_NOTINSTANTIATED 

Interface function not registered.

EI_API_ADP_eERR_STUB_NOTIMPLEMENTED 

Interface function not implemented.

EI_API_ADP_eERR_QOS_802_1Q_NOT_SUPPORTED 

802.1Q tagging not supported.

EI_API_ADP_eERR_QOS_PTP_EVENT_VALUE_OUT_OF_RANGE 

DSCP value for PTP (IEEE 1588) Event messages out of range.

EI_API_ADP_eERR_QOS_PTP_GENERAL_VALUE_OUT_OF_RANGE 

DSCP value for PTP (IEEE 1588) General messages out of range.

EI_API_ADP_eERR_QOS_URGENT_VALUE_OUT_OF_RANGE 

DSCP value for CIP Urgent messages out of range.

EI_API_ADP_eERR_QOS_SCHEDULED_VALUE_OUT_OF_RANGE 

DSCP value for CIP Scheduled priority messages out of range.

EI_API_ADP_eERR_QOS_HIGH_VALUE_OUT_OF_RANGE 

DSCP value for CIP High priority messages out of range.

EI_API_ADP_eERR_QOS_LOW_VALUE_OUT_OF_RANGE 

DSCP value for CIP Low priority messages out of range.

EI_API_ADP_eERR_QOS_EXPLICIT_VALUE_OUT_OF_RANGE 

DSCP value for CIP UCMM, transport class 2/3 messages out of range.

EI_API_ADP_eERR_TCPIP_IPADDR_VALUE_INVALID 

ADP TCP/IP object error codes (base 0x38020Dxx)

IP address value is invalid or reserved.

EI_API_ADP_eERR_TCPIP_GATEWAY_VALUE_INVALID 

Gateway address value is invalid or reserved.

EI_API_ADP_eERR_TCPIP_DOMAINNAME_NULL_POINTER 

Domain name can't to be referenced with NULL pointer.

EI_API_ADP_eERR_TCPIP_DOMAINNAME_LENGTH 

Domain name length is restricted to 48 bytes.

EI_API_ADP_eERR_TIMESYNC_WRONG_FORMAT 

ADP Ethernet Link object error codes(base 0x38020Exx)

ADP timeSync object error codes (base 0x38020Fxx) Format error. Check specification for this attribute.