| uint32_t EI_API_ADP_setCmgrCb | ( | EI_API_ADP_CBCmgr | fuCallback_p | ) |
Register callback function for ForwardOpen, LargeForwardOpen and ForwardClose.
Register a callback function which is called when a request for the services ForwardOpen, LargeForwardOpen and ForwardClose was received.
| [in] | fuCallback_p | Pointer to the callback function. |
| EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_UCmgrInfo_u