EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_pruicssInit()

uint32_t EI_API_ADP_pruicssInit ( EIP_SLoadParameter ptPara_p)

Load and initialize the EtherNet/IP firmware in the PRU.

Initializes PRU and registers the interrupts given in the configuration parameters.

Parameters
[in]ptPara_pLoad parameter.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
Example
#include "EI_API.h"
uint32_t errCode;
memset (&tParam, 0, sizeof (EIP_SLoadParameter));
memmove (tParam.ai8uMacAddr, EI_APP_aMacAddr_g, 6);
tParam.pruInstance = CONFIG_PRU_ICSS1; // SysConfig definition of PRU-ICSS block instance used by stack
tParam.phy0Instance = CONFIG_ETHPHY0; // SysConfig definition of PHY0 instance used by stack
tParam.phy1Instance = CONFIG_ETHPHY1; // SysConfig definition of PHY1 instance used by stack
errCode = EI_API_ADP_pruicssInit(&tParam);
ETHIP_API uint32_t EI_API_ADP_pruicssInit(EIP_SLoadParameter *ptPara_p)
Load and initialize the EtherNet/IP firmware in the PRU.
Definition EI_API_ADP_stub.c:73
uint8_t ai8uMacAddr[EIP_MAC_ADDR_LEN]
Definition EI_API_ADP_define.h:167
Definition EI_API_ADP_define.h:166
See also
EI_API_ADP_pruicssStart EI_API_ADP_pruicssStop