EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_pruicssStart()

void EI_API_ADP_pruicssStart ( void  )

Starts the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit.

Remarks
Shall be called after EI_API_ADP_pruicssInit.
Example
#include "EI_API.h"
uint32_t errCode;
memset (&tParam, 0, sizeof (EIP_SLoadParameter));
memmove (tParam.ai8uMacAddr, EI_APP_aMacAddr_g, 6);
tParam.pruInstance = CONFIG_PRU_ICSS1; // SysConfig definition of the PRU-ICSS block instance used by the stack.
tParam.phy0Instance = CONFIG_ETHPHY0; // SysConfig definition of the PHY0 instance used by the stack.
tParam.phy1Instance = CONFIG_ETHPHY1; // SysConfig definition of the PHY1 instance used by the stack.
errCode = EI_API_ADP_pruicssInit(&tParam);
ETHIP_API void EI_API_ADP_pruicssStart(void)
Starts the PRU0 and PRU1 firmware on the PRU-ICSS block instance specified in EI_API_ADP_pruicssInit.
Definition EI_API_ADP_stub.c:123
ETHIP_API uint32_t EI_API_ADP_pruicssInit(EIP_SLoadParameter *ptPara_p)
Load and initialize the EtherNet/IP firmware in the PRU.
Definition EI_API_ADP_stub.c:73
uint8_t ai8uMacAddr[EIP_MAC_ADDR_LEN]
Definition EI_API_ADP_define.h:167
Definition EI_API_ADP_define.h:166
See also
EI_API_ADP_pruicssInit EI_API_ADP_pruicssStop