EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ EI_API_ADP_getModuleNetworkStatus()

uint32_t EI_API_ADP_getModuleNetworkStatus ( T *  pAdp_p,
EI_API_ADP_SModNetStatus_t pAdpStatus_p 
)

Get adapter status values.

This function may be called to retrieve module and network status values from the adapter.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pAdpStatus_pPointer of type EI_API_ADP_SModNetStatus_t to the adapter status structure.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include "EI_API.h"
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getModuleNetworkStatus(pEI_API_ADP, &adpStatus);
ETHIP_API uint32_t EI_API_ADP_getModuleNetworkStatus(T *pAdp_p, EI_API_ADP_SModNetStatus_t *pStatus_p)
Get adapter status values.
Definition EI_API_ADP_stub.c:468
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition EI_API_ADP_stub.c:231
General adapter status collection.
Definition EI_API_def.h:196
See also
EI_API_ADP_setModuleNetworkStatusFunc EI_API_ADP_SModNetStatus_t EI_API_ADP_EError_t