| void DIO_DEVICE_cobjTimeOutCb | ( | uint8_t * | producedConnectionPath, |
| uint16_t | producedConnectionPathLen, | ||
| uint8_t * | consumedConnectionPath, | ||
| uint16_t | consumedConnectionPathLen | ||
| ) |
Callback function for Connection Time Out.
Callback function which is called when a request for the DOP related IO Communication state of "Connection Time Out"