EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_dopSetValue()

static void DIO_DEVICE_dopSetValue ( uint16_t  instanceID,
ei_api_cip_edt_bool  value 
)
static

user function to set Discrete Output Point value

Parameters
[in]instanceIDInstance-ID of the DOP object
[in]valuethe value to be set on the output for the given instance