EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_dipGetValue()

static void DIO_DEVICE_dipGetValue ( uint16_t  instanceID,
uint8_t *  pValue 
)
static

user function to read out Discrete Input Point value

Parameters
[in]instanceIDinstance-ID of the DIP object
[out]pValuepointer to value, to be set by user