EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_DOP_receiveDataEvent()

uint32_t DIO_DEVICE_DOP_receiveDataEvent ( uint16_t  instanceID,
ei_api_cip_edt_bool  value 
)

should be called to pass I/O data to the DOP object

Parameters
[in]instanceIDinstance-ID of the DOP object
[in]valueDOP value
Returns
EI_API_eERR_CB_NO_ERROR if successful, otherwise error code