EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_DOP_init()

void DIO_DEVICE_DOP_init ( EI_API_CIP_NODE_T *  pCipNode)

Initialize DOP class.

Initializes DOP Class and its initial state.

This function creates the DOP class. The class instance contains attribute for the revision.

Parameters
[in]pCipNodePointer to the CIP node.
[in]pCipNodeCIP Node pointer