| uint32_t DIO_DEVICE_DOP_getObjValue | ( | uint16_t | instanceId, |
| uint16_t | attrID, | ||
| void * | pValue | ||
| ) |
reads the requested attribute from DOP object
| [in] | instanceID | instance-ID of the DOP object |
| [in] | attrID | attribute-ID of the DOP object |
| [out] | pvalue | DOP requested attribute will be written here |
reads the requested attribute from DOP object
| [in] | InstanceID | the instance-ID of the DIP object |
| [in] | attrID | the AttributeID to be readed out |
| [out] | pValue | pointer to save the result |
< value attribute
< Fault Action
< Fault Value
< Idle Action
< Idle value
< Run_Idle_Command
< object state