EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_DOG_init()

void DIO_DEVICE_DOG_init ( EI_API_CIP_NODE_T *  pCipNode)

Initialize DOG class.

Initialize the DOG class.

This function creates the DOG class. The class instance contains attribute for the revision.

Parameters
[in]pCipNodePointer to the CIP node.
[in]pCipNodepointer to CIP node