EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_DIP_getInputValue

typedef void(* DIO_DEVICE_DIP_getInputValue) (uint16_t instanceID, uint8_t *pValue)

function pointer prototype for reading input value

Parameters
[in]instanceIDinstance-ID of the object
[out]pValuepointer to the value