EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_DIP_addObject()

bool DIO_DEVICE_DIP_addObject ( uint16_t  instanceID,
DIO_DEVICE_DIP_ObjectCfg_t pDipConfig 
)

Create and add a DIP instance object.

Parameters
[in]InstanceIDthe instance-ID of the DIP object to be created
[in]pDipConfigconfiguration for this instance object
Returns
true if successful, otherwise false

< get-input-value function pointer is mandatory

< get-event status is mandatory in order to run the objects state-machine