EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

◆ DIO_DEVICE_CFG_getFactoryResetData()

void * DIO_DEVICE_CFG_getFactoryResetData ( void  )

Provides pointer to factory reset non volatile data.

Called by DEVICE_PROFILE_INTF_cfgGetFactoryResetData function of device profile interface. Function needs to be registered by DEVICE_PROFILE_register call.

Returns
pointer to factory reset non volatile data.
Example
#include "device_profiles/discrete_io_device/discrete_io_device_cfg.h"
{
uint32_t error = DEVICE_PROFILE_INTF_ERR_General;
if (NULL == pIntf)
{
error = DEVICE_PROFILE_INTF_ERR_PtrInvalid;
goto laError;
}
...
...
error = DEVICE_PROFILE_INTF_ERR_OK;
laError:
return error;
}
void * DIO_DEVICE_CFG_getFactoryResetData(void)
Provides pointer to factory reset non volatile data.
Definition discrete_io_device_cfg.c:548
uint32_t DEVICE_PROFILE_register(DEVICE_PROFILE_INTF_Interface_t *pIntf)
Registers discrete IO device profile interface functions.
Definition discrete_io_device.c:251
void *(* getFactoryResetData)(void)
Definition device_profile_intf_intern.h:60
struct DEVICE_PROFILE_INTF_Interface::@7 cfg
Definition device_profile_intf_intern.h:46
See also
DEVICE_PROFILE_register DEVICE_PROFILE_INTF_cfgGetFactoryResetData